Open an object
    Open an object from 
Project view
.- InProject view, double-click the object or mouse over the object and then select. 
The object opens in a separate tab if the object has a dedicated editor. 
Properties
 for the object also open.Provide Feedback