Manage graphic objects
    Create, edit, move, and delete graphic object types and instances.
Any object that you create in the default 
UI
 folder or a subfolder of the UI
 folder is automatically configured as a type. Types are available in Type view
 in the UI
 folder.Provide Feedback