Animate a graphic object
    Add and configure number, sequential, or parallel animation properties to animate an object.
- InProject view, select the object to animate.
- InProperties, at the top, selectand then select either: - Number animation. Animate objects by changing the value to another value over specific time.
- Sequential animation. Animate objects with a simple transition in the serial mode.
- Parallel animation. Animate object with a simple transition in the parallel mode.
 TIP: You can also right-click a property that supports animations and select .
- Configure animation properties. See Animation properties.
Provide Feedback