Graphic objects
    Use predefined graphic objects to add visual components to 
FactoryTalk Optix Applications
. Use Presentation Engines to display the UI at runtime on different viewports.FactoryTalk Optix Studio
 includes predefined graphic objects to add and arrange in the visual editor. See Predefined graphic objects and Editor. In 
Project view
 and in the editor, create, duplicate, edit, and set the properties of graphic object instances and graphic object types. See Manage graphic objects and Graphic objects layout.Provide Feedback