RA EtherNet/IP Station

RA EtherNet/IP Station

BrowseName
RAEtherNetIPStation
SuperType
Communication station(CommunicationStation)

Properties

Name
BrowseName
DataType
Description
Route
Route
Route to the RA EtherNet/IP Controller (for example, 192.168.1.10\Backplane\1)
Timeout
Timeout
Status variables
StationStatusVariables
Station status information.
Operation code
OperationCode
(Inherited from Communication station)
Tags
Tags
(Inherited from Communication station)
Types
Types
(Inherited from Communication station)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal