CODESYS Station
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Gateway IP | GatewayIP | IP address of a valid CODESYS Gateway available in the network; usually, the IP address of the controller. | |
Port | Port | TCP/IP port used to connect with the controller. You can obtain the value from the CODESYS PLC Programming Environment: From the On line menu, select Communication Parameter. | |
Device Name / Address | PLCAddress | The CODESYS Controller Device Name or its IP address. The IP address can refer to the same machine that runs the driver using the local IP address or localhost. | |
Provide Feedback