Web presentation engine

When a client connects at runtime to the specified web server URL, generate an interactive session for the authenticated user.
BrowseName
PresentationEngine
SuperType
Presentation engine(PresentationEngine)

Properties

Name
BrowseName
DataType
Description
Dynamic variables polling time
DynamicVariablesPollingTime
Time interval for the periodic reading of the dynamic link source field variables.
Protocol
Protocol
Protocol used for communication between web clients and the server, either https or http.
IP address
IPAddress
Server IP address. If you host the server locally, set its IP address to "127.0.0.1". Do not use the "localhost" keyword and do not include the protocol information ("http://", "https://") before the IP address.
Port
Port
Port used for communication between web clients and the server.
Hostname
Hostname
Server hostname.
Maximum number of connections
MaxNumberOfConnections
Maximum number of clients that can connect to the web server.
Start window
StartWindow
(Inherited from Presentation engine)
LoginWindow
LoginWindow
(Inherited from Presentation engine)
Style sheet
StyleSheet
(Inherited from Presentation engine)
Starting user
StartingUser
(Inherited from Presentation engine)
Session
Session
(Inherited from Presentation engine)
Sessions
(Inherited from Presentation engine)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal