UI Session

Manage the idle timeout and the interactive session locale.
BrowseName
UISession
SuperType
SessionType(SessionType)

Properties

Name
BrowseName
DataType
Description
Inactivity timeout duration
IdleTimeoutDuration
Duration of the idle timeout after which the session stops.
Inactivity timeout active
IdleTimeoutEnabled
False: in case of user inactivity in the interface, the session remains valid; True: in case of user inactivity for a certain period of time, the session stops.
IsInteractive
Native session
IsNative
True: the UI session is native, False: otherwise.
Web session
IsWeb
True: the UI session is web, False: otherwise.
User
(Inherited from SessionType)
Locale
LocaleId
(Inherited from SessionType)
Language
Language
(Inherited from SessionType)
Measurement system
MeasurementSystem
(Inherited from SessionType)
Actual locale
ActualLocaleId
(Inherited from SessionType)
Actual language
ActualLanguage
(Inherited from SessionType)
Actual measurement system
ActualMeasurementSystem
(Inherited from SessionType)
Time zone offset
TimeZoneOffset
(Inherited from SessionType)
LoggedIn
(Inherited from SessionType)
Groups
(Inherited from SessionType)
Roles
(Inherited from SessionType)
Rights
(Inherited from SessionType)

Events

IdleTimeoutEvent
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal