Presentation engine

Create interactive sessions at runtime.
BrowseName
PresentationEngine
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Start window
StartWindow
Type of start Window object to create at the start of the session.
LoginWindow
LoginWindow
Type of login Window object that is prompted at the start of the session when you are not logged in.
Style sheet
StyleSheet
Set the styles of graphical objects, either globally or for specific object classes.
Starting user
StartingUser
The starting user with which to authenticate the session.
Session
Session
Sessions
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal