Native presentation engine

At startup of the project at runtime, generate an interactive session initially authenticated with the specified user.
BrowseName
NativePresentationEngine
SuperType
Presentation engine(PresentationEngine)

Properties

Name
BrowseName
DataType
Description
Dynamic variables polling time
DynamicVariablesPollingTime
Time interval for the periodic reading of the dynamic link source field variables.
Text render type
TextRenderType
Enable virtual keyboard
EnableVirtualKeyboard
Enable/disable the virtual keyboard.
Start window
StartWindow
(Inherited from Presentation engine)
LoginWindow
LoginWindow
(Inherited from Presentation engine)
Style sheet
StyleSheet
(Inherited from Presentation engine)
Starting user
StartingUser
(Inherited from Presentation engine)
Session
Session
(Inherited from Presentation engine)
Sessions
(Inherited from Presentation engine)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal