Add Work Center
After adding the Area, the user can add the Work Center.
NOTE:
The following points are required to view data on
Work Center level dashboard
:- Data from different meters which are directly connected to a Work center node will be considered for the data aggregation.
- For consumption and demand charts, the respective resource meter has to be configured with the proper tag mapping.
- For Cost charts, the respective rate schedule should be configured at the Site level.
- For Emission, the respective emission factor should be configured at the Site level.
- For Production and energy intensity charts should have correct tag mapping for production count measurement.
- Harmonized units are defined at the Enterprise level and will be used to display harmonized consumption, intensity, or emissions data.
Perform the following steps to add a Work center under the Area:
- SelectAreafrom the hierarchy list.
- Click the [
] icon and click
Add.TheAdd New Work Center Dialog - ClickAdd.TheAdd Componentdialog box is displayed.Add Component- Work Center Dialog
- UnderNodefrom the left pane, selectWork centerand set these parameters:
- Type: Select aWork centertype from the drop-down list.Work Center Types
- Name: Provide a Work center name.
- Description: Provide a description of the Work Center.
- ClickAdd.
The "
Work center added under Area successfully
" message is displayed.The user can also export the data file to local. For more details, see Export Data File
Related Information
:Provide Feedback