Add Region
After adding Enterprise, it is necessary to add location by adding Region.
NOTE:
The following points are required to view data on
Region level dashboard
:- For Cost charts, the respective rate schedule must be configured at the Site level.
- For Emission, the respective emission factor must be configured at the Site level.
- For Production, energy intensity charts must have correct tag mapping for production count measurement.
- For more than one resource meter harmonized unit defined at the Enterprise level will be used for displaying data for consumption, intensity, and emission.
NOTE:
The user can also export the data file to local. For more details, see Export Data File.
Perform the following steps to add a Region under Enterprise:
- Select theEnterprisefrom the hierarchy list.
- Click the [
] icon and click
Add.TheAdd Newdialog box is displayed.Add New Region Dialog - ClickAdd.TheAdd Componentdialog box is displayed.Add Component
- UnderNode, clickRegionand set these parameters:
- Name: Provide a Country or Region name.
- Description: Provide a description of the Region.
- ClickAdd.
The "
Region added to hierarchy successfully
" message is displayed.Related Information
:Provide Feedback