LCD module overview
The 2080-LCD is an external text display that is optional for a
Micro810
LC10 controller. The 2080-LCD contains a 1.5-inch LCD and a keypad. The 2080-LCD functions
as:- A backup memory module forMicro810LC10 controllers.
- A simple Human Machine Interface.
- The configuration tool for the Smart Relay function blocks.
Configure the LCD module with one of the following methods:
- Use theFactoryTalk Design Workbenchsoftware.
- Use the main menu and LCD on the 2080-LCD module.
IMPORTANT:
The 2080-LCD module supports
FactoryTalk Design Workbench
programs or Smart Relay function blocks.- If you download a program usingFactoryTalk Design Workbench, the download process overwrites any Smart Relay function block instructions.
- If you restore the Smart Relay functions using the main menu on the 2080-LCD module, the restore process overwrites theFactoryTalk Design Workbenchprogram.
For more information about the 2080-LCD module, the Smart Relay function blocks, and the wiring instructions, see Micro810 Programmable Controllers User Manual (publication 2080-UM001).
Provide Feedback