Back up project files to an LCD module
The 2080-LCD module functions as a backup memory module for
Micro810
LC10
controllers.Use the
Back up to the LCD module
button on the LCD
Module
configuration page to write the user programs and function files to the
LCD module. The button is available when the Micro810
LC10 controller is in
Remote program
mode.Prerequisites
- TheMicro800controller is inRemote programmode.
To back up project files to an LCD module
- InProject Organizer, double-click the controller to open the controller application workspace.
- In theControllertree, selectLCD Module.
- On theLCD Moduleconfiguration page, selectBack up to the LCD module.
- InMemory module, selectBack up.
Provide Feedback