Restore project files from the LCD module
The 2080-LCD module functions as a backup memory module for
Micro810
LC10
controllers.Use the
Restore from the LCD module
button on the LCD Module
configuration page to restore project files from the LCD module to the FactoryTalk Design Workbench
project.Prerequisites
- TheMicro800controller is inRemote programmode.
To restore project files from the LCD module
- InProject Organizer, double-click the controller to open the controller application workspace.
- In theControllertree, selectLCD Module.
- On theLCD Moduleconfiguration page, selectRestore from the LCD module.
- InMemory module, selectRestore.
Provide Feedback