Replace a currently assigned variable

Use the variable selector to replace the variable that is currently assigned to a Program Organization Unit (POU) element with a different one.
Prerequisites
To replace a currently assigned variable
  1. In the language editor, right-click the variable, and then select
    Select variable
    .
  2. In the variable selector, do one of the following:
    • Select another variable, and then select
      Select
      .
    • Double-click another variable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal