Variable selector

Use the variable selector to manage project and program variables.
By default:
  • Opening the variable selector from the language editor of a program displays the local variables of the current program.
  • Opening the variable selector from the language editor of a user-defined function or user-defined function block displays the global variables in the project.
  • Opening the variable selector from a
    Micro800
    controller configuration page displays the global variables in the project.
In the variable selector:
  • Use breadcrumbs to navigate variable scopes.
  • On the
    <controller-name>
    page, double-click a link to view variables for that scope.
    Variable selector -
  • Select beside the controller name to select a scope and view variables for that scope.
    Variable selector - Scope list
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal