Configure Tableau to Connect to a Virtual PostgreSQL Data Interface

This egress data interface is exposed as a virtual PostgreSQL server that emulates a real Postgres server, and it currently supports Tableau Desktop and Tableau Server. This section explains how to connect these tools to a virtual PostgreSQL data interface. After the configuration is performed and the connection is established, users can run SQL queries directly from supported tools.
NOTE:
For more information on Cognite-related documentation, please refer to Assets tag and Timeseries tag.
NOTE:
In all BI tools, it is recommended to use the sorting functionality of the tool to arrange data in ascending or descending order.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal