Prerequisites

  • Tableau Cloud/Desktop is installed. For more information, refer to Download Tableau.
  • License for Tableau Cloud/Desktop.
  • Postgres JDBC driver is installed, refer to Driver Installation.
    NOTE:
    The driver should be installed on the machine that will run the Tableau Desktop client to connect Tableau with the PostgreSQL server.
  • Access to
    FactoryTalk DataMosaix SaaS
    .
  • Register the application using the Machine-to-Machine type in
    FactoryTalk DataMosaix SaaS
    . For information on registering an application in
    FactoryTalk DataMosaix SaaS
    , refer to Register Application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal