Supported Versions
The following Tableau versions are supported by virtual Postgres interface:
- For Tableau Server, the supported version is 2024.2.2.
- For Tableau Desktop, the supported version is 2024.2.2.
- For Tableau Cloud, the supported version is 2024.2.0.
Provide Feedback