Default Capability Groups
The following table displays the list of default capability groups and the associated capabilities with applied actions. When you create a new project in
FactoryTalk DataMosaix SaaS
, these capability groups are generated by default. There are 20 default capability groups. You can choose the required capability group from the list based on your requirements and the capabilities and actions applied to it.The
UPDATE
capability is not available for FTDM-Grp-Project in order to prevent modifying or removing any OpenID connect-related configuration.If the default capability group does not fulfill your requirements, you can create a custom capability group to suit your needs. To create a custom capability group, refer to Create a new Capability Group.
NOTE:
Default groups have predefined capabilities, and these capabilities are not modifiable.
No | Default Capability Group Name | Capabilities with applied actions |
|---|---|---|
1 | FTDM-Grp-3D | threedAcl: read | create | update | delete |
2 | FTDM-Grp-AccessManagement | groupsAcI: read | list, extractionPipelinesAcI: read | write |
3 | FTDM-Grp-Applications | datasetsAcI: read | write, filesAcI: read | write. dataModelsAcI: read, dataModellnstancesAcI: read |
4 | FTDM-Grp-Chart | assetsAcI: read, timeSeriesAcI: read, filesAcI: read, groupsAcI: list, projectsAcI: list, dataModelsAcI: read, dataModellnstancesAcI: read |
5 | FTDM-Grp-CogniteApilnputValidations | datasetsAcI: read |
6 | FTDM-Grp-ContextDiag | filesAcI: read | write, assetsAcI: read | write, eventsAcI: read | write, labelsAcI: read | write |
7 | FTDM-Grp-ContextEntity | entitymatchingAcI: read | write, assetsAcI: read, timeSeriesAcI: read | write |
8 | FTDM-Grp-Data | timeSeriesAcl: read, rawAd: read | write, eventsAcI: read | write, assetsAcI: read | write, relationshipsAcI: read | write, filesAcI: read write, sequencesAcI: read | write, transformationsAcI: read | write, sessionsAci: create, projectsAci: list, groupsAci: list, datasetsAci: read | write |
9 | FTDM-Grp-DataModel | dataModelsAcl: read | write, dataModellnstancesAcI: read | write |
10 | FTDM-Grp-DataSetsManagement | rawAcI: read | write | list, datasetsAcI: read | write |
11 | FTDM-Grp-Experimental-Human | scheduledCalculatlonsAd: read | write, monitoringTasksAd: read | write, timeSeriesSubscriptionsAcI: read | write, hostedExtractorsAd: read | write, workflowOrchestrationAcI: read | write |
12 | FTDM-Grp-Experimental-Machine | scheduledCalculationsAd: read | write, monltoringTasksAcI: read | write, timeSerlesSubscrlptlonsAcI: read | write, hosted ExtractorsAcI: read | write, workflowOrchestrationAcI: read | write |
13 | FTDM-Grp-Extractor | timeSeriesAcl: read | write, rawAcI: read | write | list, eventsAcI: read | write, extractionRunsAcI: read | write, extractionConfigsAcI: read | write, assets Acl: read | write, relationshipsAci: read | write, datasetsAci: read, filesAci: read | write, sequencesAcI: read | write extractionPipelinesAcI: read | write, transformationsAcI: read | write, groupsAcI: list, projectsAcI: list, sessionsAcI: create, dataModelsAcI: read | write, dataModellnstancesAcI: read | write |
14 | FTDM-Grp-Function | functionsAcl: read | write, filesAcI: read | write, sessionsAcI: create |
15 | FTDM-Grp-GenApplications | dataModelsAcl: read | write, dataModellnstancesAci: read | write, assetsAcI: read | write, timeSerlesAcI: read | write, filesAcI: read | write, eventsAci: read | write, sequencesAcI: read | write, labeisAci: read | write, transformationsAcI: read | write, functionsAcI: read | write, projectsAcI: read | list, rawAci: read | list | write, extractionPipelinesAcI: read | write, extractionRunsAci: read | write, extractionConfigsAci: read | write, datasetsAci: read, relationshipsAcI: read | write, sessionsAci: create |
16 | FTDM-Grp-Media | filesAcl: read, annotationsAcl: write |
17 | FTDM-Grp-Pipeline | extractionPipelinesAcI: read | write, extractionConfigsAcI: read | write, extractionRunsAcI: read |
18 | FTDM-Grp-Project * | projectsAcI: read | list |
19 | FTDM-Grp-Raw | rawAcI: read | write | list |
20 | FTDM-Grp-ViewApp | projectsAcI: list, dataModelsAcI: read, dataModellnstancesAcI: read, extractionPipelinesAcI: read, extractionConfigsAcI: read |
It is not recommended to update or delete any OpenID connect-related configuration after the project has been created. Because of this, the UPDATE capability of the FTDM-Grp-Project is removed in order to limit access to OpenID connect.
Provide Feedback