Capability Groups

A capability is the ability to interact with a specific resource or feature. It can be defined as a collection of specified capabilities with applied actions. To control access to data and features, you can define what capabilities users or applications need to work with different roles. A capability is defined by a resource type, a scope, and actions. The resource type and scope define the data the capability applies to, while the action defines the operations you are allowed to perform.
For example:
3d:create
: This capability can be used to create and upload 3D models.
timeseries:read
: This capability can be used to read a time series.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal