Configure Power BI to Connect to a FactoryTalk DataMosaix SaaS Project

This section describes how to connect to your project using Power BI connector to create reports.
NOTE:
The Power BI connector is available as a beta version. It is recommended to use virtual PostgreSQL data interface instead of this method to connect to Power BI. For more information on the virtual PostgreSQL data interface, refer to Configure Power BI to Connect to a Virtual PostgreSQL Data Interface.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal