Automatic Data Refresh of Reports in Power BI Service
Prerequisite:
- Power BI Gateway is installed, up and running.
Follow the instructions to publish report to a workspace on Power BI Service and perform the data refresh:
- In the Power BI Desktop application, navigate toHome>Publish.ThePublish to Power BIdialog box is displayed.
- Select the workspace from the list of workspaces.
- ClickSelectto publish.When publishing is complete, aPublishing to Power BIdialog box is displayed which allows you to navigate to your report on Power BI Service.Publish PowerBI
Now your Power BI Service is ready to use withFactoryTalk DataMosaix SaaSand Power BI Gateway. To learn more about data refresh, refer to Data refresh in Power BI.
Provide Feedback