View FactoryTalk AssetCentre server and agent status via FactoryTalk System Status
Portal
FactoryTalk®
System Status PortalFactoryTalk® Administration Console
. This portal is
installed with FactoryTalk® Services Platform
by selecting FactoryTalk
System Status PortalStarting from FactoryTalk AssetCentre version 16.00.00,
FactoryTalk
System Status Portal shows the server and agent status of
FactoryTalk AssetCentre
in the FactoryTalk
Directory they
share. Only one FactoryTalk AssetCentre
server is allowed in the FactoryTalk
Directory. Prerequisites
- Make sure that at least one application has been created in the FactoryTalk Directory.
To view the status of FactoryTalk AssetCentre server and
agents
- In the web browser's address bar, enter one of the following:
- http://or<ComputerName>/FTSystemStatushttps://, where<ComputerName>/FTSystemStatusComputerNameis theFactoryTalkDirectory server computer. For example,https://.<MyFTDPC>/FTSystemStatus
- http://<IPAddress>/FTSystemStatusorhttps://, where<IPAddress>/FTSystemStatusIPAddressis the IP address of theFactoryTalkDirectory server computer. For example,https://.<192.16.2.1>/FTSystemStatus
TIP:If you are signing in from theFactoryTalkDirectory server computer, you can uselocalhostto replaceComputerNameorIPAddress. For example,http://localhost/FTSystemStatusorhttps://localhost/FTSystemStatus. - PressEnter.
- Enter aFactoryTalkuser account with access to the application that you want to view and its password. Select theKeep me signed incheckbox to stay signed in until you sign out manually or until cookies stored by the website in your browser are deleted.
- SelectSign in.
- On theFactoryTalk Applicationspage, select an application.
- Hover overHost nameto view the state.
For more information, see the FactoryTalk System Status Portal
Help and
FactoryTalk Services Platform Help
. Provide Feedback