Recommended System Limits
Observe these limits, from the FactoryTalk AssetCentre reference architecture:
- The recommended maximum number of FactoryTalk AssetCentre concurrent clients that can have simultaneous access to a FactoryTalk AssetCentre server is 150.TIP:Both FactoryTalk AssetCentre concurrent clients and computers with the FactoryTalk Diagnostics Connector installation should count as part of the maximum recommended number. The FactoryTalk Diagnostics Connector option is explained in a later section.
- The recommended, maximum tested number of FactoryTalk AssetCentre agents per server is 100. Do not exceed 50 remote agents.
- The recommended, maximum tested number of FactoryTalk AssetCentre agent groups is 100. Do not exceed 50 remote agent groups.
- The recommended, maximum tested number of FactoryTalk AssetCentre agents per agent group is 5.
- The necessary number of agents per server is dependent upon the number of assets to be serviced.For estimation purposes, one agent is capable of servicing approximately 100 assets per 12 hours.For detailed information, refer to Knowledgebase Document ID: IN29429 - Determining the Necessary Number of FactoryTalk AssetCentre Agents.
- The maximum number of FactoryTalk AssetCentre servers per FactoryTalk Directory is 1. This number cannot be exceeded.
Provide Feedback