FactoryTalk Security

FactoryTalk Security authenticates user identities and authorizes user requests to access a FactoryTalk enabled system. These security services are fully integrated into the FactoryTalk Directory and are included as part of the FactoryTalk Services Platform. FactoryTalk Security includes user authentication that determines who can open, create, modify, and delete application components, and on which hosts the actions are allowed. It is also possible to use FactoryTalk Security to add user and group security accounts, as well as Windows-linked accounts, and set up security for actions such as tag writes, open, and delete.
Refer to Knowledgebase Document ID: IN36251 - FactoryTalk Security - Tips and Best Practices for more information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal