Event Log

The Event Log displays information regarding events that occur in the system. Events are generally system initiated, such as a server coming online or the completion of a scheduled task. Event records can originate from any piece of FactoryTalk software, and include the time the action was logged, from which program it was logged, and from which host it was logged.
An example of an event would be a piece of FactoryTalk software checking out an activation from an Activation server, and would include the specific information on the activation name, serial number, and type checked out.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal