Audit Log

The Audit Log displays information regarding user actions performed in the system, such as making edits to an RSLogix 5000 project or checking out a file from the FactoryTalk AssetCentre database. Audits can originate from any piece of FactoryTalk software, and include the time the action was logged, from which program it was logged, from which host it was logged, and which user performed the action.
An example of an audit would be a user going online with a ControlLogix processor and making changes. In this example, the FactoryTalk AssetCentre server would receive audits for the user going online with the processor, as well as each edit made, such as creating a tag and deleting a rung.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal