Maximum File Size
The maximum file size that can be added to the FactoryTalk AssetCentre Archive is slightly larger than two gigabytes. File additions exceeding this size limit will be automatically cancelled in most versions of AssetCentre, whereas the attempt was made and then failed in older versions (v2.21, v2.21.01 only.)
Provide Feedback