Archive to Archive Compare Clean-up
Compare Engines will extract any required files from the archive and store them locally to run the compare. Once the compare is complete, these files will remain on the local hard drive to help speed future compares. To remove these files, use
Tools > Options > Compare Configuration > Erase All
.Provide Feedback