Archive Extractor

The FactoryTalk AssetCentre Archive Extractor is available to system administrators for the purposes of archive high availability. In the event of AssetCentre Server downtime, the Archive Extractor can be used to retrieve files from archive, allowing users access to configuration files at all times. For more information on the Archive Extractor, refer to Knowledgebase Document ID: QA8254 – FactoryTalk AssetCentre Archive Extractor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal