Condition - Logged Time
How do I open the New Condition dialog box?
How do I open the Condition Properties dialog box?
- SelectView > Searches, or click theSearchesbutton.
- Select the search to contain the new condition.
- Click theConditionstab.
- Click theNew Conditionbutton.
- SelectView > Searches, or click theSearchesbutton.
- Select the search containing the condition to modify.
- Click theConditionstab and select the desired condition.
- Click
.
Use the
New Condition
dialog box or Condition Properties
dialog box to
specify or modify the content for which you would like to search. For example, create or
modify a condition that searches for log records with a specific logged time (the date the
FactoryTalk AssetCentre database received report of the event from the software product; for
example, in the last three days or between specific dates like April 7 and 14, 2007).The logged time and occurred time may be different if you disconnect from the network while
FactoryTalk AssetCentre caches data, or if the time on the server is different than the time
on your computer.
TIP:
The
Logged Time
column of data appears in the Audit Log, the Event Log, and the Diagnostics and Health Log.Provide Feedback