Add a contact or group to the list of recipients

You can add the existing contact or group to the list of recipients to receive the FactoryTalk AssetCentre notifications via email.
To add a contact or group to the list of recipients
  1. In the
    Contacts and Groups
    dialog box, select the existing contact or group you want to add to the list of recipients.
    TIP:
    You can use the
    Ctrl
    or
    Shift
    key to select multiple contacts or groups.
  2. Click the
    To
    button to add the selected contact or group to the list of recipients at the bottom of the dialog box.
    Alternatively, you can double-click a contact or group to add it to the list of recipients.
  3. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal