Delete searches
You can delete any search definition for a search you no longer want to run or schedule. Deleting a search definition removes it from the
Searches
tab and the FactoryTalk AssetCentre database. It is recommended that you do not delete a search that is in the middle of a scheduled run. Therefore, delete only inactive search definitions.Search results are emailed to a recipient list; they can also be exported and saved through the
Report
tab. Therefore, any saved results of a particular search will not be deleted with the search definition.Prerequisites
- To delete a search, you must be granted theView a SearchandDeletepermissions.
To delete a search
- SelectView > Searches, or click theSearchesbutton.
- To make a scheduled search inactive before deleting its definition, deselectActivenext to the scheduled search row.
- Select the search definition to delete. To select multiple search definitions, useCtrl-ClickorShift-Click.
- SelectEdit > Delete, or click
.TIP:You can also right-click the search row and selectDelete. - ClickYes.
Provide Feedback