Run searches immediately
Run a scheduled or unscheduled search immediately.
Prerequisites
- To run a search, you must be granted theView a SearchandExecutepermissions.
- To run a search immediately, you must be granted the appropriate permission for the type of search you are going to run -View Audit Log,View Event Log, orView Diagnostics & Health Logpermission.
To run searches immediately
- SelectView > Searches,or click theSearchesbutton.
- Select the search row.
- Click theRun Nowbutton.TIP:You can also right-click the search row and selectRun Now. The results of scheduled and unscheduled searches will open in your default browser.For manually executed searches, the results display matched records up to a maximum of 10,000 rows. If the number of matching records exceeds this limit, we recommend scheduling a search instead. Scheduled searches are not subject to the 10,000-row limit.
Provide Feedback