Compare Options dialog box for FactoryTalk View Site Edition

How do I open the Compare Options dialog box?
  1. On the
    Schedules
    tab, select a Backup and Compare schedule for FactoryTalk View Site Edition.
  2. In the lower left portion of the
    Schedules
    tab, select the asset.
  3. In the lower right portion of the
    Schedules
    tab, click anywhere in the
    Compare Options
    box and then click the browse button.
Use the
Compare Options
dialog box to specify the components of the FactoryTalk View Site Edition backup you want to include in the compare operation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal