Configuration Data Compare Partner dialog box

How do I open the Configuration Data Compare Partner dialog box?
  1. Click the
    Schedules
    button to open the
    Schedules
    tab.
  2. Select a Backup and Compare schedule for a Siemens controller or a Generic FTP Device.
  3. In the lower left portion of the
    Schedules
    tab, select the Siemens controller or Generic FTP Device.
  4. The lower right portion of the
    Schedules
    tab lists operation properties for the device. Click in the Configuration Data Compare Partner field and click browse_button_small.
Use the
Configuration Data Compare Partner
to select a version of the Configuration Data binder to compare to device data in a Backup and Compare schedule for certain device types (such as Siemens controllers, Generic FTP Devices, and Allen-Bradley PowerFlex Drive). During the Backup and Compare operation, first the device data is retrieved (and depending on the schedule settings, stored as a new backup version). Then the retrieved data is compared to the specified Configuration Data version.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal