Print log records
You can print a selected record or all of the shown records in a log.
To print log records
- SelectView > Logs, or click theLogsbutton.
- From theViewmenu, select the desired log, or click the button to show theEvent Log,Audit Log, orDiagnostics & Health Log.TIP:If Quick Search results are shown, you can also print those records by clicking theQuick Search Resultsbutton.
- Select the desired records. To select multiple records, useCtrl-ClickorShift-Click.
- Click
. - Complete theRecord Selection Optionsdialog box.
- ClickPrint.
- Complete thePrintdialog box and then clickPrintagain.TIP:Files attached to log records are not printed with log records.
Provide Feedback