About the Log Item Details pane
The
Log Item Details
pane, located below the log records, shows the same information seen in each log, but expands the Message for the log. To resize the pane, position the pointer between the log records and the top of the Details
pane, and drag the cross-bar shape up or down to make the Log Item Details
pane larger or smaller. You can copy information from the Log Item Details
pane.
: Click to change the status of a Diagnostics and Health Log record to indicate whether or not the issue has been resolved or needs to be addressed. You can also comment on a log record without changing its status. This icon is only available when you select a Diagnostics and Health Log record.
: Click to show a file attached to a log record. File attachments are generated automatically by the software product that creates the log record and may contain additional information.
Provide Feedback