Issue with security-enabled RSLogix products
Scheduled events for Allen-Bradley Logix 5000 and PLC-5 controllers would fail if FactoryTalk Security was enabled for earlier versions of RSLogix 5000 and RSLogix 5. The problem is fixed in RSLogix 5000 versions higher than 16 and for RSLogix 5 version 7.30.10.3 and higher.
This issue does not affect other devices’ schedules (such as robots or Allen-Bradley PanelView devices). If a schedule contains affected processors and other devices, the scheduled event will only fail for those affected processors for which FactoryTalk Security is enabled in the programming software; the event will complete for the other devices.
Provide Feedback