Add an Agent Group dialog box

How do I open the Add an Agent Group dialog box?
  1. If you are not in it, enter Design mode.
  2. On the
    Menu bar
    , click
    View > Agent Groups
    (or click the
    Agent Groups
    button).
  3. Click the
    Add Agent Group
    button on the
    Agent Group Creation and Agent Assignment
    toolbar.
    TIP:
    You can also right-click anywhere in the
    Agent Group Creation and Agent Assignment
    pane and select
    Add Agent Group
    .
Use the
Add an Agent Group
dialog box to create an agent group.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal