Items in the Select Group Members dialog box
Items in the dialog box include:
- Contacts/GroupsExisting contacts and groups you can add to the group. To select multiple contacts or groups, useCtrl-clickandShift-click. If the contact or group you want to add is not listed, cancel the two group dialog boxes and create the contact or create the group.
- SelectMove the selected Contacts/Groups on the left side of the dialog box to theMemberslist on the right side of the dialog box. To remove any unwanted contacts or groups, clickOKto return to theNew group namedialog box.You can also clickCancelto not add any of the selected contacts or groups.
- MembersThe contacts and groups currently included in the group.
Provide Feedback