Edit additional information to the Asset Inventory result

You can manually add details to the Asset Inventory result by editing the
Additional Information
field. Make sure the Asset Inventory backup file is checked out so that the
Asset Inventory
window is opened in editable mode. You can only edit the
Additional Information
field in editable mode.
To add details to the Asset Inventory result
  1. On the
    Devices
    tab in the
    Asset Inventory
    window, type the information in the
    Additional Information
    field. Or click additional information browse button in the
    Additional Information 1
    or
    Additional Information 2
    or
    Additional Information 3
    column. The
    Additional Information
    dialog box opens.
    TIP:
    You can change the default additional information column name
    Additional Information 1
    ,
    Additional Information 2
    , and
    Additional Information 3
    in the
    Options: Asset Inventory
    dialog box.
  2. In the
    Additional Information
    dialog box, type the information.
  3. Click
    OK
    . The additional information shows in the
    Additional Information
    column.
  4. Click Asset Inventory check in to check in changes made to additional information.
    TIP:
    The Asset Inventory undo button and the Asset Inventory check in button are available when changes are made to the additional information field. Once changes are checked in, they become unavailable.
If you want to clear the changes made to additional information, click Asset Inventory undo.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal