Change commission date to the Asset Inventory result
Commission date is the date on which an equipment, facility, or plant (which is installed, complete, or near completion) is tested to verify if it functions according to its design objectives or specifications. You can change the commission date in the Asset Inventory result by editing the
Commission Date
field. Make sure the Asset Inventory backup file is checked out so that the Asset Inventory
window is opened in editable mode. You can only edit the Commission Date
field in editable mode.To change the commission date
- On theDevicestab in theAsset Inventorywindow, click the drop-down arrow
in the Commission Datecolumn. - Browse the calender and click the date as needed.
- Click
to check in changes made to commission date.TIP:The
button and the
button are available when changes are made to the commission date field. Once changes are checked in, they become unavailable.
If you want to clear the changes made to commission date, click
.
.Provide Feedback