Items in the Configure Server Settings Utility window

The following table describes the items in the
Configure Server Settings Utility
window.
Items
Descriptions
Server Location
Specifies the fully qualified domain name (FQDN) of the FactoryTalk AssetCentre server computer or IP address where the
FactoryTalk AssetCentre
server is located.
Use the secure communication channel
Turns on TLS encryption to secure the network between the
FactoryTalk AssetCentre
components.
IIS Server communication port
Specifies the IIS Server communication port for HTTPS request. The port number is set as 443 by default. If the HTTPS port was previously configured using FactoryTalk Services Platform, such as port 4356, then the existing HTTPS port setting is retained. For more information, see Configure the IIS Server communication port for HTTPS.
Base IP Port
Specifies the base IP ports that are used for server services. Ports 7002 and 7004 are open by default.
Use the forward proxy
Configures a proxy that acts as an intermediary between the FactoryTalk AssetCentre requests and the Product Compatibility and Download Center (PCDC). For more information, see Configure the proxy for Assets Lifecycle.
System "From" Email Address
Sets the optional sender's email address.
  • If you configure this property, the testing email and email notifications will be sent from the email address.
  • If you leave it empty, the emails will be sent from a default system address.
To configure main SMTP policy settings for FactoryTalk AssetCentre, such as SMTP server address or port, go to
FactoryTalk Administration Console
>
System
>
Policies
>
System Policies
>
SMTP Policy
. For more information, see
Configure SMTP policy
in the FactoryTalk Services Platform Help.
OK
Saves the changes and closes the window.
Cancel
Exits the window.
Apply
Saves and applies the changes.
Help
Opens the Help.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal