Configure the IIS Server communication port for HTTPS
During the installation, the IIS Server communication port is set for HTTPS request. When the
Secure communication with TLS
checkbox is selected, the port number is set as 443 by default for HTTPS. You can configure the default HTTPS port as needed. When the checkbox is not selected, the port number is set as 80 by default for HTTP, and you cannot configure the HTTP port. If the HTTPS port was previously configured using FactoryTalk Services Platform, such as port 4356, then the existing HTTPS port setting is retained.To configure the IIS Server communication port for HTTPS
- On the FactoryTalk AssetCentre server computer, selectStart>Rockwell Software>FactoryTalk AssetCentre ServerSettings.
- In theConfigure Server Settings Utilitywindow, enter an unused port from 1025 through 49151 in theIIS Server communication portbox.TIP:If the specified port is blocked by the FactoryTalk AssetCentre Web Client supported browsers, you cannot access FactoryTalk AssetCentre Web Client. For more information about the browser blocked ports, see the following:
- Google Chrome: ChromeBlcokedPorts
- Microsoft Edge: EdgeBlockedPorts
- Mozilla Firefox: FirefoxBlockedPorts
IMPORTANT:
As the IIS Server communication port is specified, you cannot configure the
Primary Server Web Services Base URL
.Provide Feedback