Sign in to FactoryTalk AssetCentre Web Client

You must sign in every time you try to open the web client with a browser.
To sign in to FactoryTalk AssetCentre Web Client
  1. From the
    Start
    menu, select
    Rockwell Software
    >
    FactoryTalk AssetCentre Web Client
    , or open the browser, and then enter the URL address http://<FQDN>/RockwellSoftware/AssetCentreWebClient.
    TIP:
    FQDN
    is the fully qualified domain name of the FactoryTalk AssetCentre Server computer.
    If you have changed the default port in site binding, you need to include the self-defined port number in the computer name part in the form as
    MYSERVER:PortNumber
    .
  2. From the FactoryTalk AssetCentre Web Client page, sign in using one of these ways. Before signing in to FactorTalk AssetCentre Web Client, you need to configure
    Azure Active Directory
    ,
    Azure AD site
    ,
    OpenID Connect site
    , and
    Azure AD user group
    in the Azure portal and
    FactoryTalk® Administration Console
    . For more information, select
    Help > Contents
    from the FactoryTalk Administration Console.
    • To sign in using a Windows-linked user or FactoryTalk user account, select
      Password
      , and then enter the username and password.
    • To sign in using an Azure AD user account, select
      Azure AD
      , and then use the dropdown menu to select an Azure AD site. Clicking
      Sign in
      starts the Azure AD's authentication process.
      TIP:
      When configuring the Azure AD Authenticate Site in FactoryTalk Administration Console, you need to provide a Client Secret from the Azure AD App Registration to successfully sign in using the FactoryTalk AssetCentre Web Client and Azure Ad Authentication.
    • To sign in using an OpenID Connect Identity Provider, select
      OpenID Connect
      , and then use the dropdown menu to select an Open ID Connect site. Clicking
      Sign in
      starts the OpenID Connect Identity Provider's authentication process.
  3. Select
    Sign in
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal