Configure Idle Time-out property

When no interaction with the web client has occurred for 20 minutes, you will be automatically signed out. You can adjust the Idle Time-out property using the Internet Information Services (IIS) Manager.
To configure Idle Time-out property
  1. On the FactoryTalk AssetCentre server computer, open
    Internet Information Services (IIS) Manager
    .
  2. In the
    Connections
    pane, select
    Application Pools
    .
  3. Under
    Application Pools
    , right-click
    AssetCentreWebClient
    , and then select
    Advanced Settings
    .
  4. Do the following to configure Idle Time-out property:
    • To adjust the length of time before the user is automatically signed out:
      Adjust
      Idle Time-out (minutes)
      as desired. The default length of time is 20 minutes.
    • To prevent the user from being automatically signed out:
      Change
      Idle Time-out Action
      by selecting
      Suspend
      from the dropdown menu. The default selection is
      Terminate
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal