View properties

View detailed information of a specific device. A property icon can only be shown in the
Report
page.
Prerequisite
  • Make sure that you have the
    View Security Posture Check Dashboard
    permission.
    To configure permissions, go to
    FactoryTalk Administration Console
    >
    Policies
    >
    Product Policies
    >
    FactoryTalk AssetCentre
    >
    Feature Security
    >
    Security Compliance Policies
    .
To view device properties
  1. On
    Security Compliance
    , select the Allen-Bradley Logix 5000 controller asset or the container, and then select
    Report
    .
    TIP:
    Select the parent node will include all the devices in the parent container.
  2. Select
    Card
    or
    Table.
  3. Select the desired device, and then select . You can view device details and check which scanned results meet or do not meet your expected results. For more information, see Rule settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal